Silicon Labs’ cover photo
Silicon Labs

Silicon Labs

Semiconductor Manufacturing

Austin, TX 212,306 followers

Silicon Labs is the leading innovator in low-power wireless connectivity.

About us

Silicon Labs is the leading innovator in low-power wireless connectivity, building embedded technology that connects devices and improves lives.  Merging cutting-edge technology into the world’s most highly integrated SoCs, Silicon Labs provides device makers with the solutions, support, and ecosystems needed to create advanced edge connectivity applications. Headquartered in Austin, Texas, Silicon Labs has operations in over 16 countries and is the trusted partner for innovative solutions in the smart home, industrial IoT, and smart cities markets.

Website
https://www.silabs.com
Industry
Semiconductor Manufacturing
Company size
1,001-5,000 employees
Headquarters
Austin, TX
Type
Public Company
Founded
1996
Specialties
Energy-friendly 32-bit MCUs, wireless MCUs, and 8-bit 8051 MCUs, Wireless ZigBee, Thread, Bluetooth & Sub-GHz, Low-power Sensors, bluetooth, Matter, Zigbee, Z-Wave, Wi-Fi, Wi-SUN, and Sub-GHz

Locations

Employees at Silicon Labs

Updates

Similar pages

Browse jobs

Stock

SLAB

NASDAQ

20 minutes delay

$140.60

-0.42 (-0.298%)

Open
142.45
Low
138.83
High
142.45

Data from Refinitiv

See more info on Bing

Funding