Overview
Benefits of Electronic Shelf Labels
Electronic Shelf Labels (ESLs) enable retailers to update prices automatically, in real-time across the store, eliminating days of tedious and error-prone manual work. With ESLs, retailers can increase pricing efficiency and accuracy, optimize click and collect, and simplify replenishment. Store operators can quickly react to market prices and easily synchronize pricing to keep up with the online competition. ESLs allow customers to immediately see the correct price and get personalized, in-depth product information creating a seamless in-store and online shopping experience with price transparency.
Electronic Shelf Labels (ESLs) consist of a few main components: an e-ink display, radio, microcontroller, and batteries. Despite the simple part list, designing a high-quality, long-life ESL is not easy. Check these essential design considerations to learn more.
Maximize Reliability
Silicon Labs utilizes a large-scale test network that supports up to 1,500 nodes, enabling realistic validation of complex Bluetooth LE PAwR applications. This allows customers to test and optimize the Bluetooth performance and reliability in environments that closely mirror real-world deployments. Customers benefit with faster time market with mature solutions.
Bluetooth ESL and Silabs Support
Bluetooth Low Energy (LE) networks have long struggled to support large-scale, bidirectional communication with tiny energy drains, but the introduction of Periodic Advertising with Responses (PAwR) in Bluetooth 5.4 has transformed connectivity, enabling efficient, synchronized interactions among thousands of nodes. Silicon Labs Bluetooth SDK offers demo applications for both Bluetooth ESL and access point that provides a kick start for Bluetooth ESL development as described more in detail in AN1419. We recently tested the PAwR feature of Bluetooth 5.4, measuring the performance of an ESL sample application when deploying an ESL network of 1,100 tags. See the results of this large-scale testing network and its advancements in this blog. To see more optimized performance results please contact sales for more information.
Enable 10-Year ESL
Providing years of lifetime is one of the most challenging areas in ESL. How do you maximize the lifetime of battery-powered ESLs so that the retailer can avoid replacements and reduce the total cost of ownership (TCO)? To reach a 5-10 year lifetime for the ESL on CR2032 or CR2450 batteries the current budget is typically below 10uA. This budget needs to cover e-ink display updates, wireless communication and other features like flashing LEDs.
Silicon Labs' FG22 or BG22 SoC can meet these requirements as they have industry leading low power radio at 3.6 mA TX and 2.5 mA RX and ultra-low power (0.17 uA-1.8 uA) sleep modes. FG22 and BG22 also feature RFSENSE wake-on radio feature which allows the device to remain in its lowest power sleep mode (~170 nA) until it received a dedicated radio single to wake it up. This helps to preserve battery life, for example, between ESL manufacturing and deployment and keeps the ESL radio from transmitting, for example, during air freight.
Strengthen IoT Security on Electronic Shelf Labels
Security is an increasingly valid requirement for wireless ESL products - an adversary tampering with the pricing at the store can be costly. Silicon Labs' FG22 and BG22 wireless SoCs integrate hardware accelerated crypto ciphers, secure boot with the root of trust, preventing malware injection, secure debug lock/unlock, ARM TrustZone, and more. Safeguarding your ESLs with robust security protects the retailers' business and your brand.
Simplify ESL Radio Design
Radio design for the proprietary wireless protocols on the 2.4 GHz and sub-GHz frequency bands can be complicated. With the right tools, you can speed up ESL development, and reduce costs radically. Our Simplicity Studio IDE contains software examples that get you up to speed and other tools like the Radio Configurator provides an easy graphical user interface for modifying radio configurations at compile-time and generating specific PHY settings automatically without learning complex low-level registers. It comes with predefined PHY settings for most geographic regions. You can quickly customize various settings - including PHY, frequency bands, channel spacing, modulation type, bit rate, symbol maps, timing detection - for your application.
Learn More about Electronic Shelf Label Development
Get your ESL development right from the start - review our Application Note providing an in-depth description on how to drive an Electronic Paper Display with Silicon Labs’ Wireless SoCs.
Electronic Shelf Labels Block Diagram
Electronic Shelf Labels are built off a few main components integrated across a wireless microcontroller chipset, or module.
Find the Right Products
EFR32BG22 Series 2 Bluetooth Low Energy (SoC)
EFR32FG22 (FG22) Series 2 Proprietary Wireless 2.4 GHz SoC
EFR32FG23L Ultra-Low Power, Application-Optimized Sub-GHz SoC
Additional Products and Services
Machine Learning
Silicon Labs offers ML development tools for any level of experience and suited to your specific application.
Security
To stay secure, device makers need an underlying security platform in the hardware, software, network, and cloud.
CPMS
Custom Part Manufacturing Service allows customization of wireless SoCs, modules, and MCUs at the factory.
SDK Support
Reduce your software development costs by having support for critical security patches and bug fixes for up to 10 years.
Resources
Additional Resources and Documentation
Community
Browse technical support forums, knowledge base articles and example code.
Software Reference Documentation
Develop and prototype smarter. Get to market faster.
GitHub
Explore repositories and sample code libraries from Silicon Labs