Overview
VCP Drivers Features and Benefits
The CP210x USB to UART Bridge Virtual COM Port (VCP) drivers are required for device operation as a Virtual COM Port to facilitate host communication with CP210x products. These devices can also interface to a host using the direct access driver.
These drivers are static examples detailed in Application Note 197: The Serial Communications Guide for the CP210x.
The CP210x Manufacturing DLL and Runtime DLL have been updated and must be used with v 6.0 and later of the CP210x Windows VCP Driver. Application Note Software downloads affected are AN144SW.zip, AN205SW.zip and AN223SW.zip. If you are using a 5.x driver and need support you can download Legacy OS Software.
Downloads
Download and Install VCP Drivers
Downloads for Windows, Macintosh, Linux and Android below.
*Note: The Linux 3.x.x and 4.x.x version of the driver is maintained in the current Linux 3.x.x and 4.x.x tree at www.kernel.org.
Software Downloads
- CP210x Universal Windows Driverv11.4.012/18/2024
- CP210x VCP Mac OSX Driverv6.0.35/30/2025
- CP210x VCP Windowsv6.79/3/2020
- CP210x Windows Driversv6.7.69/3/2020
- CP210x Windows Drivers with Serial Enumeratorv6.7.69/3/2020
Legacy OS Software Versions
Driver Package download links and support information
Serial Enumeration Driver
What is the serial enumeration driver and why would I need it?
Tech Docs
- CP210x Universal Windows Driver Release Notesv11.3.08/9/2024
- CP210x VCP Mac OSX Driver Release Notesv6.0.210/26/2021
- CP210x_VCP_Win2K_Release_Notes9/3/2020
- CP210x_VCP_Windows_Release_Notesv6.79/3/2020
- Driver Serial Enum Release Notesv6.7.69/3/2020
Community & Support
Knowledge Base Articles
Browse our knowledge base articles for information about specific products.
User Forums
Browse technical questions, share your ideas, and learn more about our latest solutions.
Questions? You're in the Right Place.
Silicon Labs has an active, knowledgeable user community of engineers and developers that are enthusiastic about solving problems.