Arrow Electronics Exclusive: 50% Off xG28 Dev Kits
Now through October 31, Arrow Electronics is offering a 50 percent discount on the full line of development kits for Silicon Labs’ newly released EFR32xG28 platform. This offer is exclusive to Arrow Electronics customers and applies to Radio Board Kits, Explorer Kits, and Pro Kits to help developers get their hands on these SoCs to see what they can do. Long range networks are becoming more and more necessary across a broad range of smart home and industrial applications, and the xG28 family combines high-performance sub-GHz radios for long-range capabilities and a 2.4 GHz Bluetooth LE radio to enable new multiprotocol use cases into sub-GHz networks. These devices also feature built-in AI/ML hardware accelerators for implementing machine learning at the edge, key for long-range automation.
Visit www.arrow.com and enter the xG28 tool part number you are looking for or click on the hyperlinked product number below. Upon checkout, enter code WORKSWITH2023 to save 50%. This offer is limited to the first 100 customers/companies.
The promo code is valid for 50% off one of the following xG28 evaluation boards:·
The EFR32xG28 + 2.4 GHz Bluetooth Low Energy (LE) and +14 dBm Radio Board is designed to work with the WSTK and Pro Kit main board to support the development of wireless IoT devices based on sub-GHz and 2.4 GHz Bluetooth LE wireless protocols for Amazon Sidewalk, Bluetooth LE, Silicon Labs Connect, Proprietary, Wi-SUN, and Z-Wave. The kit includes the BRD4400C dual band radio capable of both +14 dBm 868/915 MHz and +10 dBm 2.4 GHz RF. The radio board provides complete reference design and design files.
The EFR32xG28 + 2.4 GHz Bluetooth LE and +20 dBm Radio Board is designed to work with the WSTK and Pro Kit main board to support the development of wireless IoT devices based on sub-GHz and 2.4 GHz Bluetooth LE wireless protocols for Amazon Sidewalk, Bluetooth LE, Silicon Labs Connect, proprietary protocols, Wi-SUN, and Z-Wave. The kit includes the BRD4401C dual band radio capable of both +20 dBm 868/915 MHz and +10 dBm 2.4 GHz RF. The radio board provides complete reference design and design files.
The EFR32xG28 +14 dBm + 2.4 GHz Bluetooth LE Pro Kit is designed to support the development of wireless IoT devices based on sub-GHz and 2.4 GHz protocols like Amazon Sidewalk, Bluetooth LE, Silicon Labs Connect, proprietary protocols, Wi-SUN, and WM-BUS. The Pro Kit includes the BRD4401C dual band radio capable of both +20 dBm 868/915 MHz and +10 dBm 2.4 GHz RF and the Pro Kit main board. The Wireless Pro Kit main board contains an onboard J-Link debugger with a Packet Trace Interface and a Virtual COM port, enabling application development and debugging of the attached radio board as well as external hardware through an expansion header. The xG28 Pro Kit provides all the necessary tools for developing high-volume, scalable sub-GHz wireless IoT applications.
The EFR32xG28 +20 dBm + 2.4 GHz Bluetooth LE Pro Kit is designed to support the development of wireless IoT devices based on sub-GHz and 2.4GHz protocols like Amazon Sidewalk, Bluetooth LE, Silicon Labs Connect, proprietary protocols, Wi-SUN, and WM-BUS. The Pro Kit includes the BRD4401C dual band radio capable of both +20 dBm 868/915 MHz and +10 dBm 2.4 GHz RF and the Pro Kit main board. The Wireless Pro Kit main board contains an onboard J-Link debugger with a Packet Trace Interface and a Virtual COM port, enabling application development and debugging of the attached radio board as well as external hardware through an expansion header. The xG28 Pro Kit provides all the necessary tools for developing high-volume, scalable sub-GHz wireless IoT applications.
The EFR32xG28 +14 dBm + 2.4 GHz Bluetooth LE Explorer Kit is designed to support the development of wireless IoT devices based on sub-GHz wireless protocols and 2.4 GHz Bluetooth LE. With support for mikroBUS(TM) and Qwiic connector, the Explorer Kit is ideal for rapid prototyping and software development. The board supports both 868/915 MHz and 2.4 GHz for Bluetooth LE and has onboard debugger support.
The PG28 Pro Kit is an ideal starting point for application development on the EFM32PG28 Microcontrollers. The board features sensors and peripherals, demonstrating some of the many capabilities of the EFM32PG28 Microcontroller. Additionally, the board is a fully featured debugger and energy monitoring tool that can be used with external applications.
*Promo code is valid for 50% off (1) XG28 Eval board. Eval boards available for this promotion include xG28-RB4400C, xG28-RB4401C, xG28-PK6024A, xG28-PK6025A, xG28-EK2705A, and PG28-PK2506A. Other exclusions may apply. Promo code cannot be combined with any other codes but can be added onto any free shipping promotions automatically applied at checkout. This offer cannot be applied to any order with exclusive pricing and the customer must choose one or the other at the time of placing the order. MyArrow customers are eligible for this promotion for purchases made on arrow.com only, so long as there are no specially priced items in their cart. Discount does not apply to purchases made on http://my.arrow.com nor purchases made on http://verical.com. Promo code may only be applied to one (1) transaction per customer prior to offer expiration date. Offer expires October 31st, 2023 at 11:59 PM MT. Arrow reserves the right to end this promotion at any time.