Overview
FreeRTOS Features
Although the FreeRTOS kernel is lightweight—with a Flash footprint that can, in many cases, be reduced to less than 10 kBytes—it provides all of the functionality needed for a robust, multi-tasking application. The kernel’s capabilities include the following:
Priority-based, preemptive task scheduling with support for time-slicing
Multiple dynamic memory allocation schemes to accommodate different system designs and timing needs
Indirect task communication via queues, event groups, and other kernel objects
Highly efficient direct-to-task notifications
Resource protection via mutexes, with support for priority inheritance
Built-in tracking of various per-task run-time statistics
Support for one-shot and periodic software timers
Licensing
As its name indicates, FreeRTOS can be used without paying any licensing fees. It is currently offered under the MIT open-source license. Explore additional information on FreeRTOS licensing.
Getting Started
Download and Install Simplicity Studio
The source code of the FreeRTOS kernel is available to developers through Simplicity Studio. Within Studio, you’ll find tools for easily adding the kernel to new projects, along with various FreeRTOS-based software examples. To install Studio, choose the appropriate software package below.
Hardware Support
FreeRTOS can be run on both EFR32 and EFM32 devices. Check Simplicity Studio for example projects targeting your preferred device.
Select a Software Example
Software examples allow you to quickly get FreeRTOS up and running on your board.
Follow these easy steps:
1. Plug kit in with USB; Use the port labeled DBG
2. Open Simplicity Studio
3. Select Software Examples featuring FreeRTOS (see screenshot)
Tech Docs
- AN1260: Integrating v3.x Silicon Labs Bluetooth® Applications with Real-Time Operating Systems in SDK v3.x and Higherv0.612/17/2024
- AN1264: Using Open Thread with FreeRTOS™v0.29/1/2022
- AN1265: Dynamic Multiprotocol Development with Bluetooth® and OpenThread on SoCs in GSDK v3.x and Higherv0.56/6/2024
Community & Support
Knowledge Base Articles
Browse our knowledge base articles for information about specific products.
User Forums
Browse technical questions, share your ideas, and learn more about our latest solutions.
Questions? You're in the Right Place.
Silicon Labs has an active, knowledgeable user community of engineers and developers that are enthusiastic about solving problems.