Support Policy for Gecko SDK and Simplicity SDK
Our newest embedded software platform, the Simplicity Software Development Kit (SDK), is designed specifically for our Series 2 and upcoming Series 3 devices.
The new SDK will branch from Gecko SDK and begin to offer new features that help developers take advantage of the advanced capabilities of our Series 2 and 3 products.
Our Gecko Software Development Kit (GSDK) will continue to be available for users of our Series 0 and Series 1 devices.
The Gecko SDK will continue to support all Series 0 and 1 devices with no change to the long-term support, maintenance, quality, and responsiveness provided under our software policy.
Patch Release Schedule
Every major.minor release receives a minimum of 18-months of support. Support is broken into two categories: active and maintenance.
Active
- The most recent major.minor release is the active release
- Patches may include fixes for any level of issue
- New active releases are made approximately every 6 months
Maintenance
- Releases move to maintenance when a newer release is available
- Patches include fixes for high-impact issues only
- Maintenance period lasts for approximately 12 month
Archived
- Maintenance is no longer provided
- Extended Software Maintenance Service (SEMS) may be available. See our SEMS page for details.
Long Term Support (LTS)
- An LTS release is a special release that receives maintenance support for an extended period.
SDK Extended Maintenance Service (SEMS)
- SEMS enables customers to extend maintenance of specific SDK releases. See our SEMS page for details.
1Check the release notes for the latest patch for complete list of devices supported
2GSDK 4.5 LTS will extend GSDK maintenance support for active Series 0 and 1 devices. Series 2 devices will not be supported.
3Series 3 support to be added to the latest Simplicity SDK release when publicly available
Support Policy FAQs
A supported SDK is one that is eligible for technical support from Silicon Labs, and eligible for software patches to fix issues. Technical questions on Silicon Labs hardware and software products are supported via our support forums.
There is no set schedule for patches. Patches for the active SDK release (the most recent major.minor release) may include (at our discretion) fixes for any level of issue and are likely to happen more often than patches for older releases. Patches will be made available as issues are discovered, assessed, and resolved.
High-impact issues include critical and blocker level bugs and security vulnerabilities. The level of the issue is determined by Silicon Labs based on the severity and impact to our customers and their products. Our intention is to balance the needs of all customers while providing high-quality, stable releases.
First, check the Release Notes for your software to see if it is a known issue. Next, search for solutions or report an issue in our support forums.
Free support is offered until the maintenance end date. Silicon Labs also offers an SDK Extended Maintenance Service (SEMS). SEMS enables customers to extend maintenance of specific SDK releases. See our SDK Extended Maintenance Service page for details.
SDK FAQs
Simplicity SDK is an embedded software development platform for building IoT products based on Series 2 and upcoming Series 3 wireless and MCU devices. It integrates wireless protocol stacks, middleware, peripheral drivers, a bootloader, and application examples – a production-quality framework for building power-optimized and secure IoT devices.
Simplicity SDK is a follow-on to the widely-adopted Gecko SDK. Simplicity SDK 2024.6 is very similar to Gecko SDK v4.x, building on top of the same platform with a very similar overall structure and architecture.
As Series 2 and Series 3 devices and wireless technology continues to evolve, so will the software support that Silicon Labs provides. Simplicity SDK will include development of new features supported only on Series 2 and 3 devices. Gecko SDK is a mature product that will be the long-term support option for Series 0 and 1 devices. Learn more information on device families and series.
Yes. While there are no new releases planned for Gecko SDK, there are several releases in maintenance that are eligible for patches to high-impact issues. Gecko SDK 4.4 will also be the long-term support option for Series 0 and 1 devices.
Silicon Labs remains dedicated to delivering reliable, supported, and well-maintained software for all active hardware products. The GSDK 4.5 LTS represents a long-term support release specifically tailored for Series 0 and Series 1 devices that are not supported by the Simplicity SDK. This release ensures ongoing maintenance for devices that remain active (i.e., not classified as NRND or EOL).
Yes, the Gecko SDK will continue to support the current Series 2 devices available in GSDK 4.4 until the designated maintenance end date. Moving forward, new features for Series 2 devices—and the upcoming Series 3 devices—will be introduced through Simplicity SDK releases. Customers seeking the latest features and ongoing support for Series 2 devices are encouraged to adopt or migrate to the latest Simplicity SDK release.
- You can continue using GSDK 4.4.x, as maintenance shall be provided through the maintenance end date.
- You will then need to migrate to 4.5 LTS for our long-term support and maintenance free of charge.
- Maintenance will continue so long as EFR32xG1x devices are recommended for new designs.
- This support will only provide critical bug fixes as categorized by Silicon Labs as we do today.
- If you choose not to move to 4.5 LTS, you can request a SEMS agreement to extend maintenance terms which has an associated fee.
- You may continue using GSDK 4.4.x, as maintenance shall be provided through the maintenance end date.
- You will then need to migrate to our Simplicity SDK releases for new features, capabilities and continued support.
- If you choose to stay on GSDK 4.4.x for Series 2 you can request a SEMS agreement to extend maintenance terms which has an associated fee. This support will only provide critical bug fixes as categorized by Silicon Labs.
- You are using our latest SDK and will continue to have access to our latest devices, features, fixes and improvements.
- Each release shall be supported for 18 months free of charge.
- Once the maintenance expires, you will need to migrate to the latest release of the Simplicity SDK.
- If you choose not to move to the latest Simplicity SDK release, you can request a a SEMS agreement to extend maintenance terms which has an associated fee. This support will only provide critical bug fixes as categorized by Silicon Labs.