9 Materials
Overview
This course will introduce engineers to developing IoT products that connect to the Google Ecosystem. The introduction will provide attendees with a holistic overview of the Google Ecosystem and how it will use the CHIP standard to connect devices.
CHIP and Thread:
- As a firmware developer, what are the key things I should know about Thread in the context of CHIP?
- Multiple protocols supported by CHIP
- Benefits of Thread
- How Thread plays in a chip environment
- Network topology
CHIP Example Applications on the SiLabs Platform
- Example applications run on the Silicon Labs platformCHIP Example apps currently available
- Anatomy of a CHIP application
- CHIP and Silicon Labs hardware
- How to build and run the chip example apps on the Silicon Labs platform
CHIP and the Google Ecosystem
- Integration with the Google ecosystem can go a long way to delight your customers
- LocalHome SDK Overview (as it currently exists)
- How LHSDK will be evolving for the CHIP world
- Demo of example apps running on Silicon Labs platform and integrated with the Google ecosystem
- Monitoring, debugging, logging
Google Ecosystem Training: Enabling Smart Home
-
1:45
-
40:57
-
16:37
-
24:43
-
15:38
-
20:51
-
26:47
-
4:25
-
22:52
*As of 5/11/2021 Project Connected Home over IP is now Matter. Learn more about Matter.