Bluetooth Workshop
-
12:46
-
25:01
-
33:30
-
21:38
This material is 4 of 4 in the Bluetooth 184 - Workshop (SSv5): Develop Power Optimized BLE Design Featuring PRS, ADC, and LDMA.
This Bluetooth workshop provides hands-on training and teaches users how to use Peripheral Reflex System to optimize power of an ADC design. The project uses Simplicity Studio v5 and the Thunderboard BG22. It shows how the PRS can be configured to have ADC samples stored in Memory without waking the core..
This Bluetooth workshop provides hands-on training and teaches users how to use Peripheral Reflex System to optimize power of an ADC design. The project uses Simplicity Studio v5 and the Thunderboard BG22. It shows how the PRS can be configured to have ADC samples stored in Memory without waking the core..
Overview
This is the final part of the training to introduce how to use PRS with and ADC and LDMA for low energy Bluetooth designs. This video provides an explaination for the code that is required to configure the PRS, LDMA and ADC in the project. It explains the code in the provided project files.
Language Choice:
Prerequisites:
BG22 Getting Started Workshop (Complete Lab 1)
Lab Procedure:
Develop A Power-Optimized BLE Design Featuring PRS, ADC, and LDMA
Hardware Required:
Thunderboard Kit EFR32BG22
(SLTB010A)