Curriculum (Series)

CHIP 180 - Connected Home over IP

This training on the Connected Home over IP project is to simplify development for manufacturers and increase compatibility for consumers.

2 Materials

Overview

The goal of the Connected Home over IP project is to simplify development for manufacturers and increase compatibility for consumers. The project is built around a shared belief that smart home devices should be secure, reliable, and seamless to use. By building upon Internet Protocol (IP), the project aims to enable communication across smart home devices, mobile apps, and cloud services and to define a specific set of IP-based networking technologies for device certification.  This curriculum presents Silicon Labs' development efforts within the project and demonstrates a door lock device solution built using CHIP and the Silicon Labs SDK.

*As of 5/11/2021 Project Connected Home over IP is now Matter. Learn more about Matter.

Knowledge Level:

Advanced

Knowledge Level

Advanced

Lab Procedure:

Connected Home over IP

Hardware Pre-requisites

  • BRD4170A for CHIP device
  • BRD4170A RCP Device
  • RaspberryPi3B+/4 
Software Pre-requisites
  • Studio 5 with GSDK 3.0.0 
  • WSL2(Linux) on Windows 10 for building the Demo CHIP project. (Linux/Mac Machine can also be used by user)
  • Latest Raspberry Pi OS, more instructions here
  • Simplicity Commander
  • Gecko SDK v2.7
Close
Loading Results
Close