Video Material

BLE-123: Lab - Out-of-the-box Thunderboard BG22 Project

This material is 2 of 6 in the Bluetooth 181 - Workshop (SSv4): Develop a Secure IoT Device on a BG22 Thunderboard Kit.

This Bluetooth workshop provides hands-on training and teaches users how to develop and deploy ultra-low-power, secure Bluetooth connectivity with the BG22 with Simplicity Studio v4.

Overview

The hands-on lab for the first day helps get the user set up with the Simplicity Studio Version 4 tool suite. The user learns how to create a project, set GATT parameters and then flash/program the Thunderboard BG22.

Lab materials are available for users to follow along with the instructor in this video.

0:00 / 0:00
Close
Loading Results
Close