WEBINAR

ZGB-201: What is Zigbee Direct?

Learn about Zigbee Direct and why you should consider developing for its ecosystem.

Overview

Watch this demo and review of Zigbee Direct, a new proposed standard that creates a tunneling protocol between Zigbee and Bluetooth devices without the need for additional gateway hardware.

Zigbee networks are widely used in smart homes because of their size, scalability and on account of the product interoperability that the protocol provides. 

Unfortunately, not all smart voice assistants offer a built-in Zigbee hub, which means that a separate piece of hardware is required to get the added user experience provided by the assistant.

The goal of this technical demonstration is to show developers how it is possible to design a system that can support the Zigbee protocol while using Bluetooth that is already available in smart devices. We will also go over other techniques and topics, such as commissioning devices, device-to-device protocol, and user control of devices.

Duration

45 Minute Presentation

Level

Intermediate

Suggested Kit

Moderator

Silabs sylvain cormier ww 2021

Sylvain Cormier

Sr. Product Marketing Manager
Silicon Labs

Speakers

Silabs marius munder ww 2021

Marius Munder

Principal Architect
Silicon Labs

0:00 / 0:00
Close
Loading Results
Close