Silicon Labs SiWx917 Wi-Fi 6 SoC Tested to Deliver Robust Connectivity and Multi-year IoT Battery Life

03/07/2025 | Kalevi Ratschunas | 4 Min Read

Battery life is one of the first characteristics buyers compare on wireless IoT devices. The longer it is, the better. According to the interoperability and power consumption test done by Novus Labs, the SiWx917 Wi-Fi 6 SoC proved to deliver robust, energy-efficient connectivity even in extreme congestion scenarios. As a result, SiWx917 was estimated to provide smart locks with up to 5 years of battery life, giving device makers an invaluable competitive advantage. Read this blog to learn more about SiWx917 power consumption, throughput, and battery life in different network congestion scenarios.


Wi-Fi IoT Devices and Connected Sleep Mode

Wi-Fi IoT devices such as smart locks, security cameras, and sensors spend most of their time sleeping while being also associated to the Wi-Fi access point (AP) and connected to the cloud. This so-called connected sleep mode (a.k.a. WLAN associated mode) reduces IoT device’s power consumption and extends battery life while keeping the device reachable from the Wi-Fi network, i.e., the cloud application and user can start data communication with the device whenever needed. Typically, the active communication period lasts just seconds or minutes after which the device resorts back to the connected sleep mode. Because of the very “sleepy” IoT duty-cycle, the device’s ability to stay connected to the Wi-Fi AP at a low power consumption in the connected sleep mode is the most critical factor affecting how long the device’s battery lasts.


SiWx917 Wi-Fi 6 SoC

Silicon Labs SiWx917 Wi-Fi 6 SoC is renowned for its exceptional energy efficiency. Its 22µA power consumption for Wi-Fi 6 connected sleep mode (TWT 60s) is among the lowest in the industry. Its combined system power for Wi-Fi 6 connected sleep and MCU is just 37µA. That’s less than any other Wi-Fi product in this market segment at the time of writing.

However, measurements in ideal conditions with a single Wi-Fi AP do not give the full picture of energy efficiency. Wi-Fi channel congestion and AP models can affect interoperability and power consumption.

To get a more holistic view on how SiWx917 performs in different network congestion scenarios, how it interoperates with different AP models, and how these aspects translate into battery-life, we hired Novus Labs, the global independent wireless engineering specialist house, to put SiWx917, our flagship Wi-Fi 6 SoC through their most rigorous wireless test program.


SiWx917 Wi-Fi Interoperability and Power Consumption Test

The purpose of the test was to find out how well SiWx917 performs in terms of connection robustness, power consumption, and throughput across 100 popular, globally used Wi-Fi AP models.

For each AP a 25-minute test was conducted to measure robustness and power consumption under different network congestion levels: 0%, 20%, 40%, 70%, 90% - 5 min each. The end-results have been tabulated by Novus Labs and can be used by IoT device makers evaluating Silicon Labs SiWx917 as a measure of robustness to compute battery life under various real-life conditions and predict variations across APs in their use case.


The following sections cover the three tests conducted by Novus Labs:

Test 1: SiWx917 Power Consumption in Standby Associated Mode

Novus Labs’ test 1 measured the power consumption of SiWx917 in the standby associated mode (connected sleep). It was conducted over multiple weeks against 100 APs with a 1-sec listen interval (DTIM10) and 55-sec MTTQ keep alive (no TWT). The results clearly show that SiWx917 sustains its superb energy efficiency across the tested APs, even under the harshest channel congestion scenarios.

The graph below shows the average current consumption for each congestion scenario (0%...90%) tested across all the Wi-Fi 4 (802.11n) and Wi-Fi 6 (802.11ax) APs with a 1-sec listen interval (DTIM10) and 55-sec MTTQ keep alive.

Results: The average power consumption in the clean channel scenario was just ~90µA while the ‘close to saturation’ traffic scenario power consumption resulted in ~217µA, which is still highly efficient considering extreme channel congestion. All tests were passed with 0 disconnects.

Siwx917 wi fi 6 soc novus labs independent test results fig1


Test 2: SiWx917 Power Consumption in Standby Associated Mode with TWT

SiWx917 is a Wi-Fi 6 (802.11ax) enabled wireless MCU and packs many advanced energy-optimizing features such as the Target Wake Time (TWT). It can determine when and how frequently to wake up to transmit and receive data, reducing power consumption and boosting battery life. In test 2, Novus Labs measured SiWx917 connected sleep power consumption in the five congestion scenarios with 10 APs using 30 sec TWT latency and 55 sec MQTT keep alive interval.

The test results clearly show the sheer efficiency advantage of SiWx917 with TWT – the average power consumption was just 49µA in the ‘clean channel’ scenario and 74µA in the ‘close to saturation’ traffic scenario.

Compared to the test 1 results (DTIM10), TWT decreased power consumption by 45% in the clean channel scenario. In the close to saturation scenario, TWT power consumption of SiWx917 was just 1/3 of the DTIM10 power consumption. In conclusion, SiWx917 with TWT can dramatically increase battery life for IoT devices, especially in congested networks.

Siwx917 wi fi 6 soc novus labs independent test results fig2


Test 3: SiWx917 Throughput

In test 3, Novus Labs tested Wi-Fi TCP TX throughput of SiWx917 with Bluetooth LE co-existence. (SiWx917 has also a Bluetooth LE radio onboard.) The Wi-Fi / Bluetooth LE co-existence throughput was measured while a smartphone was paired and connected-idle. As the results verify, SiWx917 was able to achieve a maximum throughput of 36Mbps in a ‘clean channel’ scenario and maintained a robust 6Mbps throughput even in the ‘close to saturation’ scenario.

Siwx917 wi fi 6 soc novus labs independent test results fig3


Smart Lock Battery Life Estimation with SiWx917

SiWx917 is a highly IoT-optimized Wi-Fi solution delivering extremely low power consumption in connected sleep mode to extend IoT battery life. To quantify the impact of channel congestion on battery life, Novus Labs calculated estimations for two scenarios:

  • a low-congestion scenario of a single-family home with wireless traffic generated by a television and a few smartphones and laptops
  • a high-congestion scenario mimicking multi-user dwellings such as apartments, hotels, enterprises, offices, and retail spaces.

The battery life estimations are based on 4x Energizer Lithium AA cells providing 3000mAh at 6V.

Results: Novus Labs estimated that SiWx917 can give a smart lock a long battery life that ranges from ~3 years in the high-congestion scenario with 1 sec latency and 55 sec application handshake to even up to ~5 years with TWT 30sec in the low-congestion scenario.

Siwx917 wi fi 6 soc novus labs independent test results fig4

Check full calculation details on Novus Labs’ SiWx917 Wi-Fi Interoperability and Power Consumption Test report.


Conclusion of SiWx917 Wi-Fi 6 SoC Novus Labs Test

Battery life is one of the most critical buying criteria for IoT devices. For consumers, -longer battery life means less battery replacements, less recharging, less waste, and lower costs. For industries and enterprises, longer battery life means OPEX savings: fewer site visits and system outages due to depleted batteries on sensors. The above Novus Labs test clearly evidences the unrivalled ultra-low-power advantages of SiWx917, giving up to 5 years of battery life for a smart lock, without compromising wireless performance, computing, security, and other crucial IoT capabilities.

Kalevi Ratschunas
Kalevi Ratschunas
Senior Product Marketing Manager
Close
Loading Results
Close