Video Material

EML-101: Benefits of Enabling Artificial Intelligence & Machine Learning on the Edge

This material is 1 of 3 in the Works With 2021: TinyML and Edge Machine Learning.

Explore the fundamentals of Edge Machine Learning, the benefits and steps needed to build a complete tinyML application.

Overview

Over the next few years, AI and ML (which is a subset of AI) are expected to pervade the Internet of Things (IoT). This session explains why and how you should take advantage of the movement.

During this session, we look at the benefits of enabling AI and ML on the edge and how developments in this area are driving market trends. To cater to this, Silicon Labs is addressing the challenge of running machine learning models on wireless SoCs – we’ll show you where these can be put to the best use.

0:00 / 0:00

Level

Beginner

Moderators

Silabs paul daigle ww 2021

Paul Daigle

Industrial Automation Product Manager
Silicon Labs

Silabs mansa rao ww 2021

Manasa Rao

Senior Applications Engineer
Silicon Labs

Speakers

One tech yasser khan ww 2021

Yasser Khan

CEO
ONE Tech

Silabs samuel smalling ww 2021

Samuel Smalling

Channel Partner Manager
ONE Tech

Duration

45 Minutes
Close
Loading Results
Close